SDP/SI adds a 9-axis swiss lathe to their CNC machining centers
Press Release | April 29, 2013 | New Hyde Park, NY
SDP/SI adds a Star CNC high precision Model SR-20R IV Swiss type automatic lathe ensures an uninterrupted tool path, reducing program processing time
Stock Drive Products (ISO 9001 + AS9100 Registered) is proud to announce the addition of the Star CNC high precision Model SR-20R IV Swiss type automatic lathe to their extensive CNC machining center capabilities. The machine is specially equipped with a 12’ bar feeder to perform complex machining functions. The 27-position tool station can accommodate up to 41 tools to yield a variety of tooling options and ensures an easy and flexible tooling layout. This new bar machining center has a capacity range of up to 20 mm (.79") in diameter.The included Star Motion Control System ensures an uninterrupted tool path, reducing program processing time. The sub spindle employs a spindle motor with output power equivalent to that of the main spindle to ensure improved results. In addition, the power-driven attachment motor for cross milling and backworking has improved output horsepower.
SDP/SI is a leading manufacturer of small mechanical components, servicing a wide variety of aerospace, medical and commercial industries for over 50 years. Quotes, online orders, and 3D CAD Models are available on our updated estore at https://shop.sdp-si.com/catalog. SDP/SI offers over 130,000 small mechanical components, including gears, belt and chain drives, shafts, shaft accessories, bearings, couplings, universal joints, vibration mounts, miscellaneous components, hardware, gearheads and speed reducers, right angle drives, brakes and clutches, motors and gearmotors. For additional information about SDP/SI please visit sdp-si.com.
Stock Drive Products / Sterling Instrument (SDP/SI), 2101 Jericho Turnpike, P.O. Box 5416, New Hyde Park, NY 11042-5416. Phone: 1-800-819-8900 | 516-328-3300 • Fax: 516-326-8827.