SDP/SI Logo SHOP ONLINE (800) 819-8900
    Press Releases   Miniature In-Line Slip Clutches From SDP/SI

Miniature In-line Slip Clutches from SDP/SI

Press Release  |  August 5, 2013  |  New Hyde Park, NY

Unique multi-plate designed slip-clutches which allows the output end to disengage at a predetermined torque value, preventing damage to the driven component.

Six miniature slip clutches offered by Sterling Instrument feature a unique multi-plate design that allows the output end to disengage at a predetermined torque value, preventing damage to the driven component.

Identified as the S98CA6-... series, the clutches feature a knurled adjusting nut that allows the user to set the slip torque at the desired value.  Tightening the nut compresses a spring, which presses the friction pads against the driving plates.  The clutch is constructed so that when the slip torque is reached, the input plates will slip but the output plates will not, preventing the exceeded torque from being transmitted to the output shaft.

These clutches are ideal for compact applications requiring tension control of paper, film, wire, etc.  Examples include paper handling, packaging equipment, conveyors, and textile machinery.  The series has a torque range of 0.3 to 1200 ozf. in., based on continuous operation at 50 rpm for 25 million cycles.

SDP/SI is a leading manufacturer of small mechanical components, servicing a wide variety of aerospace, medical and commercial industries for over 50 years. Quotes, online orders, and 3D CAD Models are available on our updated estore at https://shop.sdp-si.com/catalog. SDP/SI offers over 130,000 small mechanical components, including gears, belt and chain drives, shafts, shaft accessories, bearings, couplings, universal joints, vibration mounts, miscellaneous components, hardware, gearheads and speed reducers, right angle drives, brakes and clutches, motors and gearmotors. For additional information about SDP/SI please visit www.sdp-si.com.

Stock Drive Products / Sterling Instrument (SDP/SI), 2101 Jericho Turnpike, P.O. Box 5416, New Hyde Park, NY 11042-5416. Phone: 1-800-819-8900 | 516-328-3300 • Fax: 516-326-8827.